OpenCV for Microcontrollers?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OpenCV for Microcontrollers?

2,576 Views
matthiasroedder
Contributor III

Hey guys!

I'm using the K64f and I wanted to ask if there is any possibility to use OpenCV functions on it?

I've also heard of an alternative "OpenVx". Does someone has experience with this or other alternatives?

Thanks in advance!

Matthias

Tags (2)
3 Replies

2,464 Views
constantinrazva
NXP Employee
NXP Employee

Hello [email protected] ,

On this community we mainly handle questions regarding MATLAB/Simulink and our toolboxes. We currently do not have any support for openCV for the Kinetis family. I would suggest you ask on the Kinetis Microcontrollers community - there you should find help with this topic :smileyhappy:.

Kind regards,

Razvan.

2,464 Views
matthiasroedder
Contributor III

Hello @Constantin Razvan Chivu,

okay thank you for the tip :smileyhappy:

Kind regards,

Matthias

2,464 Views
constantinrazva
NXP Employee
NXP Employee

[email protected] you are welcome! Hope you find all the answers you need there.

Kind regards,

Razvan.

0 Kudos
Reply