NXP S32k144 OpenSDA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP S32k144 OpenSDA

2,091 Views
Yannalnawafleh
Contributor I

I have designed a NXP S32k144-based PCB, and I need to know if there is a programmer board that contains OpenSDA so that I can upload a Simulink model to my PCB.

Any ideas?

0 Kudos
Reply
2 Replies

2,060 Views
Edward69
Contributor I

Using the USB Multilink probe https://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320180&productTab=1/West Penn Power Customer Service You can use one of the USB Multilink probes compatible with ARM devices here. For now, you cannot use it directly from Simulink, so you have to take the generated .elf file and flash it with the S32DS, but we will add such support in the near future.

Thanks a lot for the reply. I will try the suggested solution from your link.

 

0 Kudos
Reply

2,086 Views
mariuslucianand
NXP Employee
NXP Employee

Hello @Yannalnawafleh ,

I don't if there is any dedicated external OpenSDA board, but what you can do is modify an S32K144 evaluation board to behave as an external probe just like is described in this thread: https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MCSXTE2BK142/m-p/1078629

There are also two more options:

1. Using the USB Multilink probe https://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320180&productTab=1 You can use one of the USB Multilink probes compatible with ARM devices here. For now, you cannot use it directly from Simulink, so you have to take the generated .elf file and flash it with the S32DS, but we will add such support in the near future.

2. Another option is to use the USB2Serial converter to download the code via Serial. But still, you have to first flash the bootloader inside the MCU using a JTAG probe, and to have available on your design the same UART serial connection on the S32K144 EVB to the OpenSDA.

Let me know if one of the above options fits your needs and if you have other questions as well.

Hope this helps,

Marius

0 Kudos
Reply