NXP Model-Based Design Toolbox for S32K1xx version 4.1.0 ,error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP Model-Based Design Toolbox for S32K1xx version 4.1.0 ,error

2,064 Views
642142357
Contributor III

download "NXP Model-Based Design Toolbox for S32K1xx version 4.1.0" ,error.no checkbox to download see accessory.

0 Kudos
Reply
1 Reply

1,976 Views
Daniel_Popa
NXP Employee
NXP Employee

The Web interface has been changed after release. Just click on the products, download the file as a zip (default) and then once the download is finished and you have the file on your PC, you will need to change the file extension from *.zip -> *.mltbx

The *.mltbx is the file extension required by MATLAB to start the installation process automatically.

Best regards,

Daniel

0 Kudos
Reply