NXP Model-Based Design Toolbox for MPC57xx V3.0 - Licence Faliure

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP Model-Based Design Toolbox for MPC57xx V3.0 - Licence Faliure

2,981 Views
abhishek_kumar1
Contributor IV

Hello All 

I have downloaded NXP Model-Based Design Toolbox for MPC57xx V3.0.

MATLAB Vesrion : 2018b

Windows 7 (64 bit).

I have placed the licence in(installation folder) : C:\MATLAB\2018b\AddOn\Toolboxes\NXP_MBDToolbox_MPC57xx\lic

When I try to compile, I get following Error

License Error: -1, Model-Based Design Toolbox License Missing, please go to The Model-Based Design Development Toolbox Web Site to get a free license or request a demo. Provide the following HostID: XXXXXXXX
Error evaluating 'InitFcn' callback of block_diagram 'gpio_mpc574x'. Callback string is 'mbd_mpc574x_consistency_checks(bdroot(gcs));'
Caused by:
  • MBD Toolbox configuration check error 

Licence File

#Model-Based Design Toolbox for MATLAB/Simulink - Model-Based Design Toolbox
#for MPC57xx Automotive Microprocessors Family for XXXXXXXXX Software
#Account
# License for DISK_SERIAL_NUM=XXXXXXXX xxxxxxx
INCREMENT MC_Toolbox_574xP freescale 1.0 permanent uncounted \
VENDOR_STRING="Model-Based Design Toolbox for MPC57xx \
Automotive Microprocessors Family" \
HOSTID=DISK_SERIAL_NUM=XXXXXXXX ISSUER="Freescale \
Semiconductor" ISSUED=19-feb-2019 ck=215 SN="FSL - 25918467" \
TS_OK SIGN="0279 8CFC 17A3 20A0 A975 2646 D438 39D7 E606 5F43 \
857C 6CF1 B906 77CE 671A 10E7 AE0E 5B66 8F02 B11A 9D17 7DDF \
5B92 748E EF07 CF43 494C C78F BCE2 0BBF"

Please provide a feedback. 

Labels (1)
2 Replies

2,703 Views
mariuslucianand
NXP Employee
NXP Employee

Hello [email protected]‌,

Well all of our licenses tests were successful, so please perform one of the following checks:

1. Be sure that the HostiD(Volume Serial Number) is correct. You can check it by typing the "volc" command in cmd. If is wrong please generate a new license using the correct HostID. 

2. Be sure that you saved the license from nxp website by using the "Save all" button and not copied it because it can have the .txt hidden extension.

3. Please check if the license has the .dat extension please chenge it .lic file. 

Hope this helps, 

Marius

2,703 Views
abhishek_kumar1
Contributor IV

Hello

After I changed my user name to capital letter, it works, while generating the licence.

Thanks