Motor Devkit GD3000- reg

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Motor Devkit GD3000- reg

849 Views
rajangingee
Contributor I

hi, 

i was able to run the motor using devkit GD & S32k144 with linik motor from the PMSM open loop model available in s32MBD toolkit

while i reduced my speed to zero & then starting again, i found the motor stall & after that my motor doesnt run (this was done using MATHWORKS example (FOC for PMSM with hall sensor using MCSPTEAK144) - where the host model sends speed reference via serial communication)

observed that Motor DEVKIT gets heaten up & im also getting continuity between all capacitors & Q2 mosfet - all terminals are shorted i think. the board gets heated & my D2 LED is blinking 

im getting only 0.5 to 1.2V between the terminals of D2

note: the trimpot in DEVKIT is rotated CCW to its max position  

please advice me to proceed further 

0 Kudos
Reply
0 Replies