Motor Control Class: Lecture 6 - Commutation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Motor Control Class: Lecture 6 - Commutation

14,628件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

In this sixth lecture of the motor control course we discuss about how motor phase commutation works and how can we build a commutation table to ease the software processing to compute the PWM sequence that controls the power inverter which turn the rotor. 

 

Main topics:

    - How the rotor turns when voltage is applied;

    - How to define the commutation table;

    - How to control the power inverter switches;

    - How to identify the commutation sequence;

 

Objectives:

    - Understand the concept of 6-step commutation;

    - Design the commutation vector table;

    - Understand how to operate the power inverter;

    - Test your knowledge with a short quiz;

(マイビデオを表示)

NOTE: Chinese viewers can watch the video on YOUKU using this link

注意:中国观众可以使用此链接观看YOUKU上的视频

1.JPG2.JPG3.JPG

(マイビデオを表示)

NOTE: Chinese viewers can watch the video on YOUKU using this link

注意:中国观众可以使用此链接观看YOUKU上的视频

4.JPG6.JPG

Additional information:

    - pdf attached with slides shown in these videos;

3 返答(返信)

13,044件の閲覧回数
jimduanva
Contributor II

dumitru-daniel.popa

I have tried a few  different orders of Phase A/B/C and Hall 1/2/3. The result communication table had different pattern as yours; is that all right?

If it's true, what's the main reason to cause the pattern difference?

Thanks,

Jd

0 件の賞賛
返信

13,048件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hi jimduanva‌,

It's true! So this is a very important step in making the BLDC motor working. In fact over last weekend i had to redue the procured for a another motor in order to make it run.

Initially, i thought to save some time and started to play with the CW and CCW tables manually hoping to find a quick setup to work. I managed to spin the motor but very oddly. At some point i've decided to repeat the procedure shown in this lecture and in less than 1h i had the motor running correctly and honestly the commutation tables were totally different than what i was trying to guess.

Here is a good application node that describes in details this procedure.

https://www.nxp.com/docs/en/application-note/AN4413.pdf 

Hope this helps!

Daniel

0 件の賞賛
返信

13,049件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

To test your knowledge or to have a discussion starting point let us have this short quiz session:

Q1: What is the name of the PWM technique used in this lecture to control the power inverter MOSFETs?

Q2: What are the main benefits of this PWM technique?

Leave your comments below.

Thank you!