Matlab 23b and S32K3x4EVL-T172

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Matlab 23b and S32K3x4EVL-T172

778 Views
AlexG124
Contributor II

I used Matlab/Simulink (version 23a) to build a simple model to make the RGB LEDs flash on a eval board (S32K3x4EVB-T172). This also works. Now I have updated Matlab to version 23b and have also partially renewed or updated the toolboxes. The model is still compiled correctly and flashed on the board but unfortunately the LED does not flash.
Even a simple FreeMaster example no longer runs with version 23b.

Are there any problems with the BSP?

0 Kudos
Reply
0 Replies