MPC5744P DSPI example,A vital problem occurs.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC5744P DSPI example,A vital problem occurs.

1,871 次查看
秦祥林秦
Fresh Out Contributor

When I use the MPC5744P DSPI examples, I find a problem.DSPI initialization process in the skip DISAB_IRQ (), directly into the DSPI_init.However, when the shield DSPI_init, the program has returned to normal.The initial value of the DSPI is not passed, and the default value becomes all 0.

0 项奖励
回复
1 回复

1,723 次查看
Daniel_Popa
NXP Employee
NXP Employee

Hello, 

This community is about issues encountered with the Model-Based Design Toolboxes. As far as i can see from your attachment you are using stand-alone examples for MPC5744P.

Since you are not using Matlab/Simulink to generate the code automatically for DSPI on MPC5744, my suggestion to you is to ask this on a different community: MPC5xxx or the place you have took the examples from.

Thank you!

Daniel 

0 项奖励
回复