MPC5643xL: Return to default flash configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5643xL: Return to default flash configuration

1,921件の閲覧回数
borja_heriz
Contributor I

Dear all,

I have an issue with the flash configuration of a MPC5643L.
I think that I have overwritten boot registers or something like that because when I try to download an .elf file into the flash memory it works properly (I can see a CAN message). But after a power-off cycle, the application doesn’t restart because I cannot see the CAN message anymore.
Could you please let me know the procedure to go back to the default configuration of the flash?

Thanks in advance,
Borja

0 件の賞賛
返信
2 返答(返信)

1,835件の閲覧回数
borja_heriz
Contributor I

Dear Marius-lucian Andrei,

No, I just jtagged the elf using S32 IDE. 

And yes, I'm sure that I've selected FLASH option as target memory.

Any clue about what could be happening?

Regards,

Borja

0 件の賞賛
返信

1,835件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello [email protected]‌,

So, If I understand correctly you are using the RappId Bootloader to download the code over CAN and the application is working correctly until restart. Are you sure that you have selected the flash and not the ram for target memory? What Matlab version are you using?

Best Regards,

Marius 

0 件の賞賛
返信