MCToolBox example project "adc_pdb_trigger_s32k14.mdl"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCToolBox example project "adc_pdb_trigger_s32k14.mdl"

4,183件の閲覧回数
fengwang
Contributor I

Hi Radu,

     I use MCToolBox example project "adc_pdb_trigger_s32k14.mdl" , occur this error . Could you help me kill this error ?

pastedImage_1.png

 Thanks !

Regards,

     Feng

0 件の賞賛
返信
3 返答(返信)

3,867件の閲覧回数
raduivan
NXP Employee
NXP Employee

Hi Feng,

   Please delete and remake the link between ADC block and output port. From the screenshot you attached, the error occurs because those two blocks are not connected.

Best regards,

Radu

0 件の賞賛
返信

3,867件の閲覧回数
fengwang
Contributor I

Hi Radu,

     Thank you for me to solve error  again and again.

     I installed the "Motor Control Toolbox" again , i building the project in the simulink ,occur this error  :

pastedImage_1.png

i can't understand the "setting  up the target compilers" like this ; How can i  do it follow this .

pastedImage_2.png

 Many many thanks !

Best regards,

Feng

0 件の賞賛
返信

3,867件の閲覧回数
raduivan
NXP Employee
NXP Employee

Hi Feng,

   First you need to install the compiler you intend to use and after you need to set an Environment variable which will point to the installation folder. Let me know if you need more information.

Best regards,

Radu

0 件の賞賛
返信