MBDT installer for S32S HCP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MBDT installer for S32S HCP

2,997件の閲覧回数
curt_hillier
NXP Employee
NXP Employee

Hi, I'm trying to install the HCP 1.0.0 EAR, and when downloading the *.mltbx, I get a zip file containing a directory structure with various files, but no *.mltbx.  

Flexera link:  Design : Product Download : Files (flexnetoperations.com)

File I'm trying to download:  SW32_MBDT_HCP_1.0.0.EAR_D2111.mltbx

File I actually download: SW32_MBDT_HCP_1.0.0.EAR_D2111.zip

Contents of the file I downloaded: 

C:\mw_hcp_1_0_0\SW32_MBDT_HCP_1.0.0.EAR_D2111>dir
Volume in drive C has no label.
Volume Serial Number is 48D5-EB3A

Directory of C:\mw_hcp_1_0_0\SW32_MBDT_HCP_1.0.0.EAR_D2111

11/06/2021 08:24 AM <DIR> .
11/06/2021 08:24 AM <DIR> ..
11/06/2021 08:24 AM <DIR> fsroot
11/06/2021 08:24 AM <DIR> metadata
11/06/2021 08:24 AM 159,068 [Content_Types].xml
11/06/2021 08:24 AM <DIR> _rels
11/06/2021 08:24 AM <DIR> _xmlsignatures
1 File(s) 159,068 bytes
6 Dir(s) 49,176,612,864 bytes free

 

There is no  SW32_MBDT_HCP_1.0.0.EAR_D2111.mltbx in the zip file.

0 件の賞賛
返信
2 返答(返信)

2,990件の閲覧回数
curt_hillier
NXP Employee
NXP Employee

I found the answer on the download page:

"The NXP Model-Based Design Toolbox is delivered as a MATLAB MLTBX file. If your browser download the file as a zip, simply change the file extension back to *.mltbx to be recognized by MATLAB Installer"

 

This issue can be closed.

0 件の賞賛
返信

2,974件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hi @curt_hillier,

Indeed, there is a limitation with the hosting platform I guess, for the mltbx file it downloads the installer as zip. But, by just changing the extension back to mltbx, MATLAB can recognize the file and install the toolbox as you may have already proceeded.

Regards,

Marius 

0 件の賞賛
返信