MBDT for S32K3 v 1.6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MBDT for S32K3 v 1.6

1,392件の閲覧回数
osama_desoqi
Contributor II

Hello

After installing the Model-Based Design Toolbox for S32K3 version 1.6.0. In my MATLAB model R2023b, I got a warning as shown 

Warning: An error occurred while evaluating the rtwTargetInfo file "C:\Users\win10\App-Data\Roaming\Math-Works\MATLAB Add-ons\Toolboxes\NXP_MBDToolbox_S32K3\mbdtbx_s32k3\coder-target\2021a\rtwTargetInfo.m": 'NXP S32K3xx' has been created in R2021a and is not compatible with this release of MATLAB. Please recreate the target in R2023b before attempting to
register or use the target.

 I don't know how to solve this to work the toolbox without issues .

my regards  

タグ(1)
0 件の賞賛
返信
1 返信

1,365件の閲覧回数
robertv
NXP Employee
NXP Employee

Hello @osama_desoqi ,

I tried to replicate your scenario, but unfortunately I did not manage to encounter the same issue.

Did that warning show up immediately after installing the Toolbox, or during some specific operation like building a model?

Could you please tell us more about your setup? For example:

  • How did you go about installing the Toolbox? Did you download it directly through nxp.com or did you use the Support Package available as a Matlab Add-on to install it?
  • Are you using the latest version of Matlab 2023b?
  • Have you previously installed any other version of Model Based Design Toolbox?

I noticed that in the warning you attached, the path contains a folder named "coder-target", which is unusual since the folder is called "codertarget" in our Toolbox. Was there any phase of the installation where this was modified? 

Please do not hesitate to mention anything else that you think is specific to your setup and that could help us in diagnosing the issue you have encountered.

Regards,
Robert V

0 件の賞賛
返信