MBDT for RDBESS772BJBEVB evaluation board and MC33772C IC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MBDT for RDBESS772BJBEVB evaluation board and MC33772C IC

747件の閲覧回数
Rasoul
Contributor III

We are currently using the NXP 1500V BMS evaluation board (RD-BESS1500BUN), along with NXP's model-based design tools (MBDT) in MATLAB/Simulink to develop our BMS software. Since configuring BMS IC specifications using MBDT is quite complex, we would greatly appreciate your guidance or the provision of a more complete example model that includes the secondary features.

  1. As with the RD-BESS1500BUN, the MBDT example for the RDBESS772BJBEVB only activates basic features.
    Specifically:
    • Several high-voltage measurement ports (four positive and two bipolar inputs) are not accessible in the MBDT model.
    • The board also supports precharge resistor temperature monitoring using an external sensor, but MBDT blocks for this feature are missing.

Could you please provide guidance or updated MBDT examples that include these features? Thank you sincerely for your continued support and assistance.Regards
Rasoul

タグ(2)
0 件の賞賛
返信
0 返答(返信)