MBD_freemaster problems

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MBD_freemaster problems

ソリューションへジャンプ
5,607件の閲覧回数
haoxue1027
Contributor V

Hello

What is the meaning of  coefficient a=9.5492965964254 in the demo "PMSM_ClosedLoop_mpc5744p"freemaster?

In addition, Whether to use scalar values uniformly in the MBD demo?

Any help will be appreciated.

Best regards

hao

 

ラベル(1)
0 件の賞賛
返信
1 解決策
5,587件の閲覧回数
adriantudor
NXP Employee
NXP Employee

Hi @haoxue1027 ,

This coefficient represents how many rotations per minute is 1 rad/sec. The reason o using it is due to the method of speed measuring using hall sensors ( Speed_and_Position_Estimator  block). 

Best regards,

Adrian

元の投稿で解決策を見る

4 返答(返信)
5,588件の閲覧回数
adriantudor
NXP Employee
NXP Employee

Hi @haoxue1027 ,

This coefficient represents how many rotations per minute is 1 rad/sec. The reason o using it is due to the method of speed measuring using hall sensors ( Speed_and_Position_Estimator  block). 

Best regards,

Adrian

5,587件の閲覧回数
haoxue1027
Contributor V

Hello,Adrian

Thanks you for replying.

In addition , Is the  a=0.005,Execution Time same meaning?

haoxue1027_0-1599489797776.png

best regards

hao

0 件の賞賛
返信
5,557件の閲覧回数
adriantudor
NXP Employee
NXP Employee

Hi @haoxue1027 ,

 

This coefficient multiplied with "profile_buffer" variable it represents the time base of the timer used by the Profiler block. I think there is a mistake if you found this coefficient 0.005. 

As you can see the Unit of this variable is shown as "usec" microsecond. That means the frequency of the timer used by Profiler is 1/0.000000005 = 200Mhz(so many zeros because of usec Unit). 

 

Best regards,

Adrian

5,532件の閲覧回数
haoxue1027
Contributor V

Hello,Adrian

Thank you very much.

It is helpful for me.

best regards

hao

0 件の賞賛
返信