Does anyone know about error "Undefined function 'slsfnagctlr' for input arguments of type 'char'"?
I got it during code generation of every example of MBD Toolbox S32K, using Matlab2017b. Do you think that is a Matlab incompatibility issue?
Thanks in advance!
Original Attachment has been moved to: test_adc.slx.zip
解決済! 解決策の投稿を見る。
Hi dumitru-daniel.popa,
It's working now with toolbox v 3.0.0.
Thank you very much for your support!
Regards,
Alessandro
dumitru-daniel.popa , We're facing a similar issue with the MCT Toolbox for the MPC564xL. It works with 2017a but not 2017b for similar reasons. Would there be a fix for this? If yes, when can I expect it? If no, can we have a workaround?
Hello,
We are currently working on a workaround to enable older toolboxes for running into the newer versions of the MATLAB 2017b and 2018a. Currently the fix is under testing on MPC564xL but we had some issues with the lack of HW to test on.
Stay tuned - the fix will be soon available.
Thank you for your patience and for using the tools.
Best regards,
Daniel
thank you for your reply. I have tagged you in another question. Please help me with that.
Hi alessandropintabona,
I presume you are using the toolbox v2.0.0 right ? That does not have the support for 2017b release because the Matlab changed the API. It works only until 2017a.
But, yesterday we launched v.3.0.0 version that is fully supported in 2017b: https://community.nxp.com/docs/DOC-335555
Perhaps you can upgrade to this one.
Best regards,
Daniel
Hi dumitru-daniel.popa,
It's working now with toolbox v 3.0.0.
Thank you very much for your support!
Regards,
Alessandro