Hidumitru-daniel.popa,
Recently,i am learning the dual motor demo board C-code for MPC5643L,I am combing the control process,now i have a question about it:
I right click the mouse on the function 'void FOC_Fast_ISR(void)' .I jump into a segment c-code in the file named INTCISRVEC_table.c:
#ifdef IRQ_206_FCN /* ISR 206 Equal to FOC_Fast_ISR() */
(tU32)&IRQ_206_FCN,
#else
(tU32)&dummy,
#endif
then Right the 'IRQ_206_FCN' in the INTCISRVEC_table.c
jump into a segment c-code in the file named MPC5643L_appconfig.h:
#define IRQ_206_FCN FOC_Fast_ISR
But i Right The FOC_Fast_ISR in the MPC5643L_appconfig.h,it can not jump,
I have a question that ,Where can i find the address of FOC_Fast_ISR ?
it shouldn't like as #define FOC_Fast_ISR 0x12xx xxxx xxxx ?