How to debug the MBD generated code in the S32 Design Studio using PEmicro debugger?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to debug the MBD generated code in the S32 Design Studio using PEmicro debugger?

Jump to solution
3,218 Views
rafael_barbosa
Contributor IV

Hello,

I am using the Devkit MPC5744P and the Model Based Design Toolbox 3.0.0.

I would like to debug the generated code on the target microcontroller using the PEmicro debugger.

What are the steps to import the generated code in the S32 Design Studio in order to run the debugger?

Kind Regards, Rafael

mariuslucianandrei‌

0 Kudos
Reply
1 Solution
3,099 Views
rafael_barbosa
Contributor IV

Hello mariuslucianandrei‌

I could use the PEmicro debugger for MBD generated code by importing the project.xml file generated by the MBD toolbox into the S32 Design Studio.

 

pastedImage_1.png

Kind Regards, Rafael

View solution in original post

2 Replies
3,053 Views
tl007
Contributor III

Dear @rafael_barbosa 

For some reason, i did the same but was not able to proceed with flashing the new project imported.

Can you maybe provide the next steps?

https://youtu.be/PjFWds2M4nQ

 

0 Kudos
Reply
3,100 Views
rafael_barbosa
Contributor IV

Hello mariuslucianandrei‌

I could use the PEmicro debugger for MBD generated code by importing the project.xml file generated by the MBD toolbox into the S32 Design Studio.

 

pastedImage_1.png

Kind Regards, Rafael