HotFix: MBD Toolbox rev3.0.0 for S32K

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HotFix: MBD Toolbox rev3.0.0 for S32K

4,958件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

HotFix_1: Fix FTM Initialization trigger issue

NXP Tracking number: AST-897

Problem: If you use PDB Config block and select Trigger Input Source TRGMUX_PDB_TRIG and as Input signal for External trigger FTM0 Internal Trigger, the program will encounter some building errors.

 

Root Cause: Coding building error

 

Workaround:  Update the files attached in the following folders 

{Toolbox install dir}\NXP_MBDToolbox_S32K1xx\code\mbdtbx_s32k14\mbdtbx_s32k14\  folder mbd_s32k14_ec_toolbox.mdl file

{Toolbox install dir}\NXP_MBDToolbox_S32K1xx\code\mbdtbx_s32k14\mbdtbx_s32k14\mscripts\pdb\ folder mbd_s32k14_trgmux_get_trgsrc_enum.p file

{Toolbox install dir}\NXP_MBDToolbox_S32K1xx\code\mbdtbx_s32k14\mbdtbx_s32k14\mscripts\pdb\ folder mbd_s32k14_trgmux_get_param.p file.

 

Customer Report: BUG report

Special thanks to xmwang‌  for testing and fix confirmation.

ラベル(1)
2 返答(返信)

3,949件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

HotFix_3: Fix Profiler block error

 

NXP Tracking number: AST-935 

 

Problem:  Profiler_s32k14 block fails to build - gt_pf.c: error: 'LPIT0' undeclared (first use in this function) LPIT_DRV_StartTimerChannels(0, LPIT0->SETTEN | (1 << 3))

 

Root Cause: Coding error

 

Workaround:  Update the files attached in the following folders 

{Toolbox install dir}/code/mbdtbx_s32k/mscripts/profile/mbd_s32k_profile_code.p

{Toolbox install dir}/code/mbdtbx_s32k14/mbdtbx_s32k14/blocks/profiler/profiler_s32k14_fcn.tlc

{Toolbox install dir}/code/mbdtbx_s32k14/src/c_library/gt_pf.c

{Toolbox install dir}/code/mbdtbx_s32k14/src/includes/gt_pf.h

Note: The profiler example provided will work if you choose another PIT Channel (other than 0) as it is used as Step Tick Timer.

3,949件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

HotFix_2: Fix PDB Config block - TRGMUX initialization error

 

NXP Tracking number: AST-904 

 

Problem: If you use PDB Config block for instance 1, the TRGMUX initialization parameters were wrong (only instance0 of TRGMUX available on S32k1x).

 

Root Cause: Coding error

 

Workaround:  Update the files attached in the following folders 

{Toolbox install dir}\NXP_MBDToolbox_S32K1xx\code\mbdtbx_s32k14\mbdtbx_s32k14\blocks\pdb  folder pdb_s32k14_config.mdl file

Customer Report:  Bug report

 

Special thanks to xmwang‌ for reporting this issue.

0 件の賞賛
返信