HotFix: MBD Toolbox S32K v4.1.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

HotFix: MBD Toolbox S32K v4.1.0

4,564 次查看
constantinrazva
NXP Employee
NXP Employee

Cumulative patch:

 

As you know, we're only giving out cumulative patches for a while now - they come in the form of self-extracting zips and contain all the patches, up-to-date. A user can install at any point in time the latest patch and get all the patches from before, regardless if he had or had not installed some previous patch.

 

Usage:

 

Run NXP_MBDToolbox_S32K1xx_4.1.0_patch_1.exe and enter the following path when prompted:

{YOUR_INSTALL_DIR}\NXP_MBDToolbox_S32K1xx

e.g.: C:\Users\my_user_name\Documents\MATLAB\Add-Ons\Toolboxes\NXP_MBDToolbox_S32K1xx

Note: for older versions of MATLAB, you might have the toobox installed in {ROOT}\NXP_MBDToolbox_S32K1xx\code . If you have the 'code' folder generated, you must add that path. 

Most likely you will be asked if you want to overwrite some files - just click on 'Yes to All' option. This is an indicator of things going ok. If you do not get such a prompt, something is wrong with the patch / path given.

 

NXP_MBDToolbox_S32K1xx_4.1.0_patch_1 contains:

  • HotFix1 - PIL and PIL profiler issues
  • HotFix2 - LPUART receive block - size (input) not working
  • HotFix3 - Migration of models from older version (2018.R1) not working for some .slx models

As we get more fixes in, we'll update both the list and the executable file you need to install here.

标签 (1)
标记 (5)
0 项奖励
回复
1 回复

4,003 次查看
mariuslucianand
NXP Employee
NXP Employee

 

Run NXP_MBDToolbox_S32K1xx_4.1.0_patch_2.exe and enter the following path when prompted:

{YOUR_INSTALL_DIR}\NXP_MBDToolbox_S32K1xx

e.g.: C:\Users\my_user_name\Documents\MATLAB\Add-Ons\Toolboxes\NXP_MBDToolbox_S32K1xx

Note: for older versions of MATLAB, you might have the toobox installed in {ROOT}\NXP_MBDToolbox_S32K1xx\code . If you have the 'code' folder generated, you must add that path. 

 

Most likely you will be asked if you want to overwrite some files - just click on 'Yes to All' option. This is an indicator of things going right. If you do not get such a prompt, something is wrong with the patch / path given.

 

NXP_MBDToolbox_S32K1xx_4.1.0_patch_2 contains:

  •  NXP_MBDToolbox_S32K1xx_4.1.0_patch_1 files
  • Fix support for Reference Models: all referenced models must contain our Config block
0 项奖励
回复