FreeMaster not connecting over CAN

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FreeMaster not connecting over CAN

2,697件の閲覧回数
mahdkhalid
Contributor III

Hi Dear dumitru-daniel.popa‌

I have attached the files which I built using my compiler. Please have a look.

Many thanks in advance,

Mahd

2 返答(返信)

2,449件の閲覧回数
mahdkhalid
Contributor III

Hi dumitru-daniel.popa‌,

Thank you so much for your help.

I have installed hotfix_6 and everything is working totally fine now

Best regards,

Mahd Khalid

0 件の賞賛
返信

2,449件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hi Mahd, 

Sorry for delay. I've checked the code you have sent me.

The main difference between you generated code and mine is in the flexcan_init_fnc() function:

pastedImage_1.png

Please install HotFix_6 patch in order to fix it: https://community.nxp.com/thread/451804#comment-954427 

This is a cumulative patch that fix the issue.

Please confirm you have it working. FYI, these are the HW settings i've tested with:

- 12V external power supply

- 120ohm termination resistor

pastedImage_3.png

Hope this helps!

Daniel