EPROM access

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

EPROM access

1,811件の閲覧回数
saurabhkulkarni123
Contributor II

Hello,

I want to store data in EEPROM of S32K144 NXP in MBDT, How I can store it, and how to check whether data are stored or not? Or is there any other way to store data in MBDT?

0 件の賞賛
返信
2 返答(返信)

1,752件の閲覧回数
bixby6245
Contributor I

Hello

very Informative post for storing your values you can do -

Saving a value to EEPROM
Don't write multiple values on the same address, otherwise you will lose the previously written number (unless that's what you want to do)
A memory location can only store one byte of data.
Don't write a value to the EEPROM inside an infinite loop without any delay or check for user input.

Hope so it will helps you 

dinar chronicles

 

0 件の賞賛
返信

1,785件の閲覧回数
stefancinipeanu
NXP Employee
NXP Employee

Hi, @saurabhkulkarni123 

You can check out the Flash EEPROM example from the toolbox. That example shows you how you can read and write data from/in the EEPROM memory, using Flash blocks. To visualize the data from EEPROM, FreeMASTER is used. You can find that example made for S32K144 in the following path: {toolbox_path}\src\S32_Examples\s32k14x\flash\flash_eeprom_s32k14x.mdl

Regards,

Stefan.

0 件の賞賛
返信