EEPROM Read Write

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EEPROM Read Write

2,784 Views
Partha_G
Contributor I

I am trying to write data directly to the EEPROM of S32K144 using the Flash EEERead/Write blocks  in Simulink.  I am writing the data 61H (97 in decimal) in a separate program and reading the same in another one using the FLASH blocks via CAN bus as mentioned, but I am getting the data as FF instead of 61 on the Busmaster. Please help me out.

Tags (1)
0 Kudos
Reply
2 Replies

2,748 Views
Partha_G
Contributor I

Okay! I will check, thank you!

0 Kudos
Reply

2,764 Views
Narudol-T
Contributor III

Hi,

https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Flash-EEE-Read-and-Write/m-p/1170584

you can follow this post, it solved my problem.

 

Thank you,
Narudol T.