Duty cycle

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Duty cycle

2,643件の閲覧回数
abderrahimjamao
Contributor III

Hello
in the control motor (brushless) I would like to know how the duty cycle is calculated
based on desired current and speed feedback.

regards,

Abderrahim

タグ(2)
0 件の賞賛
返信
3 返答(返信)

2,524件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

Hello [email protected],

Are you referring to a specific model from our toolbox or from a course we have here on the community? Or are you talking about some other application?

Kind regards,

Razvan.

2,524件の閲覧回数
abderrahimjamao
Contributor III

Yes , the MTRDEVKSBNK144 application. (BLDC control with s32k144 EVB).

Regards,

Abderrahim

0 件の賞賛
返信

2,524件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

Hello [email protected],

On this community we usually only answer questions regarding MATLAB/Simulink and our toolboxes; but in this case I think you are referring to the MCAT application - am I correct? If yes, adriantudor‌ can give you more details about that.

Kind regards,

Razvan.