Double PIL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Double PIL

2,294 Views
RogelioCano
Contributor I

Is it possible to run 2 PIL models in a single project? Or any other way to have multiple microcontrollers in a simulation?

0 Kudos
Reply
3 Replies

2,168 Views
Fili
Contributor I

Hi @mariuslucianand,

I'm also interested on applying multiple target processor in one Simulink session. Do you know if this is possible?

Thank you in advance.

0 Kudos
Reply

2,288 Views
mariuslucianand
NXP Employee
NXP Employee

Hello @RogelioCano

The current framework for the S32K1 allows you to deploy only the subsystem running in PIL mode on the MCU to be tested, while the inputs and send, and algorithms outputs are received via a single Serial communication. So I would say that this is now possible.

Can you please provide more details about your usecase?

Regards,

Marius

2,278 Views
RogelioCano
Contributor I

I'm currently working in MATLAB 2017B with two S32k144 connected to the computer through USB ports and I want to run both independently.

RogelioCano_1-1714147815300.png

But when I try to compile that project the next error occurs:

RogelioCano_0-1714146875541.jpeg

 

0 Kudos
Reply