Hello,
I want to program the Kinetis MKV10Z64xxx microcontroller using the Motor Control Toolbox for Kinetis V in simulink. In the target list under Target MCU Config i can select only the MKV10Z32xxx and the MKV10Z16xxx series. The MKV1xZ64xx and MKV1xZ128xxx series are not in the list, so can not be programmed.
Question
- Is there another way to select the MKV1xZ64xx and MKV1xZ128xxx series, or is this simply not possible?
- If not, is it planned for the future to support these series?
- If both false, is there a work-around?
Best Regards,
Theo