Change CAN Baud Rate in S32K3 Board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Change CAN Baud Rate in S32K3 Board

1,780 Views
embedded_will
Contributor I

Hi Community,

I'm new to MBDT and working with the S32K344. I'm setting up a basic CAN communication between the S32K344 and CAN Analyzer.

The default settings are for 1 Mbps, but I need to run the CAN at 500 kbps. Which parameters should I adjust in the S32 Configuration Tool to achieve this?

Appreciate your help—thanks in advance!

Tags (2)
0 Kudos
Reply
1 Reply

1,620 Views
Irina_Costachescu
NXP Employee
NXP Employee

Hello @embedded_will 

I would like to point you to an article describing the available options and parameters for configuring CAN peripheral inside S32CT, for S32K344. Here, you could find as well useful information on the Baudrate configuration.

Please let us know if the information in this article helps, or if further details are required from our side.

https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/Communicating-over-the-CAN-Bus/ta-p/175845...

Thank you,

Irina

0 Kudos
Reply