Change CAN Baud Rate in S32K3 Board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Change CAN Baud Rate in S32K3 Board

1,783件の閲覧回数
embedded_will
Contributor I

Hi Community,

I'm new to MBDT and working with the S32K344. I'm setting up a basic CAN communication between the S32K344 and CAN Analyzer.

The default settings are for 1 Mbps, but I need to run the CAN at 500 kbps. Which parameters should I adjust in the S32 Configuration Tool to achieve this?

Appreciate your help—thanks in advance!

タグ(2)
0 件の賞賛
返信
1 返信

1,623件の閲覧回数
Irina_Costachescu
NXP Employee
NXP Employee

Hello @embedded_will 

I would like to point you to an article describing the available options and parameters for configuring CAN peripheral inside S32CT, for S32K344. Here, you could find as well useful information on the Baudrate configuration.

Please let us know if the information in this article helps, or if further details are required from our side.

https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/Communicating-over-the-CAN-Bus/ta-p/175845...

Thank you,

Irina

0 件の賞賛
返信