Cannot connect to external mode S32K144 on R2020a

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cannot connect to external mode S32K144 on R2020a

2,567 Views
rolo90
Contributor I

Hello everyone, 

I am currently using MBDT for code gen on S32K144 eval board. I am using the lastest patch of MBDT, also I can generate code succesfully, however I am not able to connect to external mode. I have read thoroughly the posts regarding external mode like: (the path should not have spaces, tick external mode on config parameter on code generation -> interface, etc...) BUT keep getting the same error as follows:

Application BuildInfo does not exist: buildInfo.mat.

Any solutions to this?

Regards,

Rolando

0 Kudos
Reply
3 Replies

2,526 Views
rolo90
Contributor I

Hello @mariuslucianand ,

Still unable to connect. Any other solutions? May be good if you can try and share your results here.

Thanks,

Rolando

0 Kudos
Reply

2,555 Views
rolo90
Contributor I

Hello @mariuslucianand 

I have done exactly the steps shown on the link. When I clicked "Build for Monitoring", no problem application compiles and runs on the MCU, however when I click on Control Panel -> Connect I get this error: Untitled1.png

Also my configuration is:

Untitled.png

So what is the problem?

 

Thanks,

 

Rolando

0 Kudos
Reply

2,558 Views
mariuslucianand
NXP Employee
NXP Employee

Hello @rolo90 ,

Can you please try the procedure explained in the following thread?

https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/Unable-to-Deploy-and-Start-External-Mode-E...

Hope this helps,

Marius

0 Kudos
Reply