CAN FD - Master mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CAN FD - Master mode

1,202件の閲覧回数
juliana_rojas30
Contributor III

Hello community!

Can someone please confirm that the CAN FD master mode example actually works in the S32K146 board?

I configure the system to receive a CAN FD message, when it does, turn on a red LED. This works. Then, send me back a CAN FD message with a fixed ID and turn a blue LED. 

The problem occurs when I send a message with a DLC > 8, the length of the message is not received in the CAN monitoring tool,  neither does the data of the message, only the ID.

juliana_rojas30_0-1603873830118.png

Can I get some help with what might be going wrong here?

Edit: I added a picture that shows the issue.

Kind regards.

0 件の賞賛
返信
0 返答(返信)