CAN Communication Issue on S32K344 with NXP Model-Based Design Toolbox for S32K3 version 1.6.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CAN Communication Issue on S32K344 with NXP Model-Based Design Toolbox for S32K3 version 1.6.0

954 次查看
oj
Contributor I

Hello,

I am working on S32K344 and configuring CAN communication using S32 NXP Model-Based Design Toolbox for S32K3 version 1.6.0. However, I am facing an issue where I am not receiving any CAN messages on my CAN analyzer (BusMaster).

I have used the same configuration that was working perfectly in v1.5.0, but after switching to v1.6.0, the messages do not appear on the analyzer.

Details of the Issue:

  1. Setup Details:

    • Microcontroller: S32K344
    • Development Environment: S32 Design Studio
    • CAN Analyzer: BusMaster
    • Configuration: Same MEX file that worked in v1.5.0
  2. Steps I have tried:

    • Verified baud rate and CAN FD settings (matching the working setup from v1.5.0).
    • Ensured the CAN module initializes without errors.
    • Checked the message buffer configurations, which are the same as in v1.5.0.
    • .
    • Verified hardware connections, ensuring that transceiver and termination resistors are properly in place.

Request for Assistance:

  • Is there any known change in v1.6.0 that could affect CAN transmission/reception?
  • Do I need to modify any additional settings to get CAN communication working in this version?
  • Are there any debugging steps recommended to further diagnose this issue?

For reference, I am attaching my MEX file and ZIP with Simulink SLX file, which contain the configurations used.

Any guidance would be greatly appreciated.

MBDT   S32K344-WB  

Thanks!

0 项奖励
回复
0 回复数