BCC Examples using Matlab 25a

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BCC Examples using Matlab 25a

964 Views
AlexG124
Contributor II

I am trying to test an example from the BCC-Examples using Matlab 25a and the MBDT for S32K3 v1.7.0.
During migration, the configuration (S32CT) cannot be fully transferred. Unfortunately, when I try to recreate the configuration using the S32ConfigTool, I cannot see any BCC components under ‘Peripherals’.
 
Where can I find the relevant extensions and how do I install them? 

Are there any examples for the RD-HVBMSCT800BUN that work with the latest toolboxes and MATLAB 25a?

Tags (1)
0 Kudos
Reply
2 Replies

931 Views
SorinIBancila
NXP Employee
NXP Employee

Hello,

 

Unfortunately Model Based Design for BMS toolbox is not compatible with the MBD for S32K3 1.7.0. It is only compatible with S32K3 1.4.x. 

 

Best regards,

Sorin Bancila

0 Kudos
Reply

940 Views
AlexG124
Contributor II

Here some screenshots:
AlexG124_0-1779788799081.png

AlexG124_1-1779788844605.png

(and the build log)

 

Tags (1)
0 Kudos
Reply