"FSL Virtual COM Driver" certificate

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

"FSL Virtual COM Driver" certificate

2,026 Views
federicosbalchi
Contributor I

The virtual COM example in MQX 4.1 has a driver for Windows (file fsl_ucwxp.inf) that works well for Windows 7, but in Windows 8.1 it is painful to install because it's not certified by Microsoft.

We were able to install it using some dirty magic, but this involves booting windows in maintenance mode and it will not work when accessing PC remotely.

Anybody knows if there is a workaround or, better, a certified driver available?

Thanks in advance for your help.

Tags (4)
0 Kudos
Reply
1 Reply

1,530 Views
soledad
NXP Employee
NXP Employee

Hello Federico,

Please check the below thread:

https://community.freescale.com/thread/301439

Please check the answer from Ryan: " This is because of Windows 8 blocking the installation of unsigned drivers. There's a workaround, but it's a bit of a pain:

How to Disable Driver Signature Verification on 64-Bit Windows 8.1 (So That You Can Install Unsigned..."


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply