multi core platform

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

multi core platform

2,723 Views
mridulasharma
Contributor I

Hey,

Do we have any multicore platform for the MQX RTOS?

I am on a research project for real-time application on multi-core systems. I need to test some applications.

Does MQX has any support for multi-core?

please reply.

thanks

amv142

Tags (1)
0 Kudos
Reply
4 Replies

2,570 Views
RadekS
NXP Employee
NXP Employee

Hi Mridula

Yes, there is Vybrid MCU (with ARM A5 and M4 cores).

MCC code was primary developed for this MCU.

http://www.freescale.com/webapp/sps/site/homepage.jsp?code=VYBRID

BTW: Our partner TimeSys is responsible for MCC code on Linux platform. If you would like communicate between MQX and Linux systems, please contact TimeSys directly. http://www.timesys.com


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,570 Views
mridulasharma
Contributor I

Thanks RadekS

I have browsed further and got to QorIQ T4240 processor. That is a 24 core processor and I just wanna know that is it possible to have MQX support on this processor? If yes, is the MQX free or we need to but the license?

Also if T4240 is easily confiurable? I have seen some demo on youtube that shows that there can be three different applications running on three sets of 8-8 cores?

thanks

0 Kudos
Reply

2,570 Views
RadekS
NXP Employee
NXP Employee

Hi Mridula,

Unfortunately QorIQ T4240 processor isn’t between officially supported MCUs/MPUs in any MQX package.

However you could try asking our Premium Support (paid service) for help with porting to this platform.

http://www.freescale.com/pages/professional-support-for-microcontrollers:PREMIUM-SUPPORT

Please use contact [email protected] for getting more information about premium support at this platform.

Unfortunately I never worked with QorIQ T4240 processor, therefore I am not able answer your question whether T4240 is easily configurable…


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,570 Views
mridulasharma
Contributor I

Thanks it really helps

Sent from my iPhone

0 Kudos
Reply