mqx 4.2.0 supports cyassl 3.9.6 version?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mqx 4.2.0 supports cyassl 3.9.6 version?

930件の閲覧回数
sivapalana
Contributor I

Iam porting from mqx 4.0.2 to 4.2.0. So I would like to know which latest cyassl version would be compatible with mqx 4.2.0.

タグ(1)
0 件の賞賛
返信
2 返答(返信)

801件の閲覧回数
Saikiran
Contributor II

Hello Community,

we are also porting MQX 4.0 project to MQX4.2.0. In MQX4.0 project we used cyssl 3.2.0 library. 

is it possible to use cyssl 3.2.0 library in mqx 4.2 project also ? 

0 件の賞賛
返信

819件の閲覧回数
soledad
NXP Employee
NXP Employee

Hello,

MQX 4.2.0 supports the CyaSSL library version 3.3.0 .


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信