mqx 4.2.0 supports cyassl 3.9.6 version?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mqx 4.2.0 supports cyassl 3.9.6 version?

726 Views
sivapalana
Contributor I

Iam porting from mqx 4.0.2 to 4.2.0. So I would like to know which latest cyassl version would be compatible with mqx 4.2.0.

Tags (1)
0 Kudos
2 Replies

597 Views
Saikiran
Contributor II

Hello Community,

we are also porting MQX 4.0 project to MQX4.2.0. In MQX4.0 project we used cyssl 3.2.0 library. 

is it possible to use cyssl 3.2.0 library in mqx 4.2 project also ? 

0 Kudos

615 Views
soledad
NXP Employee
NXP Employee

Hello,

MQX 4.2.0 supports the CyaSSL library version 3.3.0 .


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos