lwadc calibration procedure

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

lwadc calibration procedure

1,487件の閲覧回数
goncaloandre
Contributor I

Hello,

I am trying to use the lwadc api provided with MQX 4.2.0 to read some analog inputs on the Freescale K60, but the documentation is a bit scarce and I have some doubts regarding the calibration function. I am basing myself on the sample code to read the potentiometer provided with mqx.

-Here is recommended to run the calibration procedure using ioctl, but the lwadc does not use file handles. So where should I get this file handler to each adc channel? Can't I just read/write the register (in this case bit CAL on ADCx_SC3) myself?

-Why does the sample aplication have no calibration procedure? Isn't is allways needed?

-When should I do the calibration? After _lwadc_init() and before _lwadc_init_input()?

Thanks in advance.

Goncalo

タグ(3)
1 返信

1,362件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi Goncalo:

Current BSP not support calibration, please check the init_lwadc.c file. The calibration data pointer is Null.

pastedImage_2.png

Regards

Daniel