low power modes K60N512

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

low power modes K60N512

1,336件の閲覧回数
pasini
Contributor I

I am still using TWR-K60N512 with MQX.

Datasheets says there are 10 power modes: run, wait, VLPR, VLPW, VLPS, LLS, VLLS3, VLLS2, and VLLS1

Some other datasheet also says there is a VLLS0

However, MQX just offers RUN, WAIT, STOP, VLPR, VLPW, VLPS, and LLS.

Are there VLLS3-2 modes ? Is there a VLLS0 mode ? How exactly can I configure and use them with MQX ?

That is really confusing...

My idea is that MCU is always in the lowest power consumption. When a timer (Low Power or RTC) interrupt or a button (LLWU) is pressed, interrupt routines are exectuted and MCU wakes up ( maybe at 2MHz or even lower). After executing some functions it goes back to the lowest power consumption.

I just need a timer and a pin interrupt.

Thanks in advance

Pasini

0 件の賞賛
返信
2 返答(返信)

1,203件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi

Kinetis supports several power modes (see Chapter Power Management in Kinetis reference manual).  MQX supports four basic modes (RUN, WAIT, SLEEP, and STOP).

MQX RUN operation mode is mapped on Kinetis RUN power mode by default. MQX WAIT operation mode is mapped on Kinetis VLPR power mode by default. MQX SLEEP operation mode is mapped on Kinetis WAIT power mode by default. MQX STOP operation mode is mapped to Kinetis LLS power mode by default.

For mapping, please see mqx\source\bsp\”your board”\init_lpm.c file.

low-power.jpg

Have a nice day!

Daniel

0 件の賞賛
返信

1,203件の閲覧回数
yasuhikokoumoto
Senior Contributor I

Hello Luiz,


in VLLSx modes, the wakeup from the low power mode begins with the reset sequence.

This means it would impossible to recover an execution from the point where the MCU had entered into the low power mode.

Using an OS such as MQX, the scenario might be inconvenient and those low power modes would not be supported.

If you want to use VLLSx modes, you should embed the wakeup gimmick into the OS or monitor program.


Best regards,

Yasuhiko Koumoto.

0 件の賞賛
返信