too many interrupts(gpio5_3 as interrupt source) to respond. I want to bind from cpu0 to other cpus.
I have tested it by irq_set_affinity, but it didn’t work.
last found chip->irq_set_affinity is null.now how to do it?
thanks.
Hi David
one can try to run application which uses that interrupt on specific core using examples with taskset :
in sect.6.9.4 AN12118 i.MX 8M Quad Power Consumption Measurement
or https://community.toradex.com/t/can-packets-dropped-if-high-bus-load-on-apalis-imx8-boot2qt-image-an...
Best regardsigor