Webserver running out of memory

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Webserver running out of memory

1,502 次查看
maximilianfenzl
Contributor I

Hi,

I have a problem with my http-server (MQX RTCS) running out of memory. That is what i am tried to do yet:

- I need to open 5 Sockets on the RTCS (2 of them are allways free for the webserver)

- First I created a Website ( html + separate css + separate java script file) then i recognized, that the browser is starting to crawl all linked files to the index.html at the same time. Therefore i ran into a out of memory problem, because the http server is creating a lot of tasks. Then i tried to use only one index.html file and put everything in the header of this file. This worked much better but if there are many refreshes in a short time, i also run into out of memory. 

I don´t care about the webserver running out of memory because there is no problem to restart it (not much data lost), but i need the other sockets to stay alive, so for me there is no possibility to restart the whole rtcs. It is also no problem if i don´t react to some refreshes...

Is there anybody out there, who has a Website with java + .css running and solved this problem? Is there a a setting option for the http-server to limit the creation of tasks?

Tank you so far

Max

标签 (1)
标记 (2)
0 项奖励
回复
3 回复数

1,122 次查看
karelm_
Contributor IV

Hi Max,

which version of the MQX and HTTP server do you use?

Regards,

Karel

0 项奖励
回复

1,122 次查看
maximilianfenzl
Contributor I

Hi Karel,

right now i am using MQX 4.0 and the HTTP server included.

Thanks for your answer

Regards,

Max

0 项奖励
回复

1,122 次查看
karelm_
Contributor IV

Hi Max,

I strongly recommend to wait for release of MQX 4.0.2 and port your application to it. There is new version of HTTP server in 4.0.2 (called HTTPSRV) with new API. Old server is full of bugs and memory leaks and we do not plan to maintain it (it will be removed in MQX 4.1).

Best Regards,

Karel

0 项奖励
回复