Using the Mini-Flex-Bus for external RAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using the Mini-Flex-Bus for external RAM

Jump to solution
3,753 Views
Stefan_75
Contributor II

Hi,

 

I want to use the Mini-Flex-Bus for accessing external RAM (MCF52259). There is no driver availible for this. Therefore I tried to configure the needed pins in the bsp part of the MQX system. But even there I can´t access the pins that I need for.

 

Is ther any way to solve this easily?

 

Thanks for any hint.

 

Stefan

0 Kudos
Reply
1 Solution
2,884 Views
JaimeR
Contributor III

Check this thread. That should get you started.

 

 External RAM

 

Message Edited by Jaime R on 2009-10-26 03:16 PM

View solution in original post

0 Kudos
Reply
4 Replies
2,884 Views
kleckerspur
Contributor III

link seem to be brocken !

0 Kudos
Reply
2,884 Views
kleckerspur
Contributor III

link seems to be brocken

External RAM links to ....

Welcome | Freescale Community

0 Kudos
Reply
2,884 Views
JaimeR
Contributor III

Check this thread. That should get you started.

 

 External RAM

 

Message Edited by Jaime R on 2009-10-26 03:16 PM
0 Kudos
Reply
2,884 Views
Stefan_75
Contributor II

Thanks. That´s it.

 

STefan

0 Kudos
Reply