USB mass storage support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB mass storage support

2,608 Views
kelvinho
Contributor I

I have one set of DEMOJM on my hand,

I plan to use MC9S08JM32 with assembly language my application is to make JM32 as a USB drive (e.g. drive E ; I understand JM32 only has 32K flash)

I can download few k bytes data time to time from any PC without dedicated PC software in DEMOJM kit, there are HID and CDC class examples,

 

a./ can JM32 support Mass Storage Class, is there any driver support/example ?

b./ my program is writting by assembly language, how to combine with the USB class (which are in C)

 

Thanks in advance !

 

 

Kelvin

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,017 Views
DavidS
NXP Employee
NXP Employee

The JM family is to be supported with the FSLMQX3.6 release towards the June, 2010 time frame.

It will include MSD support.

Regards,

David

0 Kudos
Reply