USB mass storage support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB mass storage support

2,610件の閲覧回数
kelvinho
Contributor I

I have one set of DEMOJM on my hand,

I plan to use MC9S08JM32 with assembly language my application is to make JM32 as a USB drive (e.g. drive E ; I understand JM32 only has 32K flash)

I can download few k bytes data time to time from any PC without dedicated PC software in DEMOJM kit, there are HID and CDC class examples,

 

a./ can JM32 support Mass Storage Class, is there any driver support/example ?

b./ my program is writting by assembly language, how to combine with the USB class (which are in C)

 

Thanks in advance !

 

 

Kelvin

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,019件の閲覧回数
DavidS
NXP Employee
NXP Employee

The JM family is to be supported with the FSLMQX3.6 release towards the June, 2010 time frame.

It will include MSD support.

Regards,

David

0 件の賞賛
返信