USB >8Gb not working properly

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB >8Gb not working properly

2,264件の閲覧回数
kalaiyarasansel
Contributor II

Hi ,

I am using MQX for my project, Where i am not able to use USB device 8GB or more than that.  If i use flash drive more than 8 GB. I could see write as success but it is not actually written into it. I tried to do flush but it is not working. I  am missing anything in the configurations. Please update me if any,

 

Thanks,

Kalaiyarasan.

ラベル(2)
タグ(2)
2 返答(返信)

2,088件の閲覧回数
kalaiyarasansel
Contributor II

Thanks, Latest MQX4.2 reslove the problem

0 件の賞賛
返信

2,088件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi KALAIYARASAN:

Could you let me know which board you are using , and echi or khci?

I would suggest you try to test this case with the latest MQX 4.2,  to see whether this issue still exist.

Regards

Daniel