USB >8Gb not working properly

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB >8Gb not working properly

2,265 Views
kalaiyarasansel
Contributor II

Hi ,

I am using MQX for my project, Where i am not able to use USB device 8GB or more than that.  If i use flash drive more than 8 GB. I could see write as success but it is not actually written into it. I tried to do flush but it is not working. I  am missing anything in the configurations. Please update me if any,

 

Thanks,

Kalaiyarasan.

Labels (2)
Tags (2)
2 Replies

2,089 Views
kalaiyarasansel
Contributor II

Thanks, Latest MQX4.2 reslove the problem

0 Kudos
Reply

2,089 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi KALAIYARASAN:

Could you let me know which board you are using , and echi or khci?

I would suggest you try to test this case with the latest MQX 4.2,  to see whether this issue still exist.

Regards

Daniel