Type definitons - mcf5225.h

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Type definitons - mcf5225.h

2,682 Views
lel_chen
Contributor I

Hi,

       The controller that I am using is MCF52259.

1) How can I read the general purpose register "D0"?

2) Is mcf5225.h the header file to be used for type definitons of the registers?

 

If YES,

--> The reset control register of M52259 is an 8 bit register, whereas, the file "mcf5225.h" specifies it as a 16 bit int.

" uint_16 RCON; // Reset Configuration Register"

 

Why is this change? Or is there a seperate header file for M52259?

 

Thanks,

Chen

0 Kudos
Reply
3 Replies

1,752 Views
JuroV
NXP Employee
NXP Employee

Hi.

 

1) What is 'general purpose register D0' ?

2) Yes, it is used also for definitions of registers.

 

Reset Configuration Register (RCON) is 16 bit wide register in mcf52259 (MCF52259 Ref. Manual, Rev. 1).

0 Kudos
Reply

1,752 Views
lel_chen
Contributor I

Sorry, my question was not about Reset Config Register[RCON], but Reset Control Register [RCR] in the reset controller module.

 

I could find it in mcf5222.h as:

------------------------------------------------------

typedef struct mcf5222_cim_struct

{

uchar RCR; // Reset control register

uchar RSR; // Reset status register

.......................

--------------------------------------------------------

 

But not in mcf5225.h

0 Kudos
Reply

1,752 Views
EAI
Contributor IV

To access D0 (or any other core processor registers) from C code, you could use inline assembly. Search for 'asm' in codewarrior help. Here is one example given in the codewarrior help:

 

long int b;
struct mystruct {
  long int a;
} ;
static asm long f(void)     // Legal asm qualifier
{
  move.l   struct(mystruct.a)(A0),D0 // Accessing a struct.
  add.l    b,D0   // Using a global variable, put return value
                  // in D0.
  rts             // Return from the function:
                  // result = mystruct.a + b 
} 
0 Kudos
Reply