Timeline view doesn't work in example, and LOG_OVERWRITE crashes CW

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Timeline view doesn't work in example, and LOG_OVERWRITE crashes CW

1,207 Views
OldPeculier
Contributor II

Hi all,

I'm testing timeline view with the example klog.c.  When I try to view, I get "No task switches found" and yet _klog_create returns MQX_OK, and _klog_control is set to the example default.  Moreover, MQX Log Summary view is showing 170 log entries under kernel logging.

Ironically it works in my application if _klog_create switch = 0.  The reason I am attempting the example is that if I set switch = LOG_OVERWRITE in my application, CW 3.8 crashes so hard I have to reboot the computer (W7).

Thanks for any help

Martin

0 Kudos
Reply
1 Reply

1,122 Views
c0170
Senior Contributor III

Hello Martin Hess,

there are missing few details, what's your target? what CW do you use? 3.8 is a version? what is the version of MQX? In order to reproduce what you have reported, we need the same configuration.

Regards,

0xc0170

0 Kudos
Reply