TWR K60 DHCP connection

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

TWR K60 DHCP connection

跳至解决方案
4,240 次查看
ralu
Contributor III

I just get tower whit K60 TWR-K60N512 processor and i succesfully compiled and run code, but I am unable to make dhcp IP retival.

 

It even does not send antyhing out (checking whit wireshark)

error is maked in source

 

 

    error = RTCS_create();    if(error)    {      printf("RTCS_create  Error %08x!\n", error);      return;    }    IPCFG_default_enet_device = DEMOCFG_DEFAULT_DEVICE;    IPCFG_default_ip_address = ENET_IPADDR;    IPCFG_default_ip_mask = ENET_IPMASK;    IPCFG_default_ip_gateway = ENET_IPGATEWAY;    LWDNS_server_ipaddr = ENET_IPGATEWAY;    ip_data.ip = IPCFG_default_ip_address;    ip_data.mask = IPCFG_default_ip_mask;    ip_data.gateway = IPCFG_default_ip_gateway;    ENET_get_mac_address (IPCFG_default_enet_device, IPCFG_default_ip_address, IPCFG_default_enet_address);    error = ipcfg_init_device (IPCFG_default_enet_device, IPCFG_default_enet_address);    if (error != IPCFG_ERROR_OK)    {      printf("Device init  Error %08x!\n", error);      return;    }    error = ipcfg_bind_dhcp_wait(IPCFG_default_enet_device, 0, NULL);    if (error != IPCFG_ERROR_OK)    {      printf("DHCP Error %08x!\n", error); //well here fails whit IPCFG_ERROR_BIND    }

 

 

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
3,315 次查看
ralu
Contributor III

It is long time ago, but issue was with powering, i dont remebere all detail, but powering oin one USB input doesnt boot eth correctly.

在原帖中查看解决方案

0 项奖励
回复
4 回复数
3,316 次查看
ralu
Contributor III

It is long time ago, but issue was with powering, i dont remebere all detail, but powering oin one USB input doesnt boot eth correctly.

0 项奖励
回复
3,315 次查看
ivanpajuelo
Contributor II

This is my Ethernet initialization code:

    void initialize_networking(_ip_address ip, _ip_address mask, _ip_address gateway, _ip_address dns, uint_32 pcbs, uint_32 msgs,

            uint_32 sockets, boolean dhcp)

    {

        int_32 error;

        IPCFG_IP_ADDRESS_DATA ip_data;

        _enet_address serverAddress =

        { 0x00, 0xcf, 0x52, 0x53, 0x54, 0xcc };

        /* runtime RTCS configuration */

        _RTCSPCB_init = pcbs;

        _RTCS_msgpool_init = msgs;

        _RTCS_socket_part_init = sockets;

        error = RTCS_create();

        if (error == RTCS_OK)

        {

            error = ipcfg_init_device(BSP_DEFAULT_ENET_DEVICE, serverAddress);

#if RTCSCFG_ENABLE_LWDNS            

            LWDNS_server_ipaddr = dns;

            ipcfg_add_dns_ip(BSP_DEFAULT_ENET_DEVICE, LWDNS_server_ipaddr);

#endif

            // check link status

            printf("\nWaiting for ethernet cable plug in ... ");

            while (!ipcfg_get_link_active(BSP_DEFAULT_ENET_DEVICE))

            {

            };

            printf("Cable connected\n");

            /* If DHCP Enabled, get IP address from DHCP server */

            if (dhcp)

            {

                printf("\nDHCP bind ... ");

                error = ipcfg_bind_dhcp_wait(BSP_DEFAULT_ENET_DEVICE, 1, &ip_data);

                if (error != IPCFG_ERROR_OK)

                {

                    printf("Error %08x!\n", error);

                }

                else

                {

                    printf("Successful!\n");

                }

            }

            else

            {

                ip_data.ip = ip;

                ip_data.mask = mask;

                ip_data.gateway = gateway;

                /* Else bind with static IP */

                printf("\nStatic IP bind ... ");

                error = ipcfg_bind_staticip(BSP_DEFAULT_ENET_DEVICE, &ip_data);

                if (error != IPCFG_ERROR_OK)

                {

                    printf("Error %08x!\n", error);

                }

                else

                {

                    printf("Successful!\n");

                }

            }

            if (error == IPCFG_ERROR_OK)

            {

                ipcfg_get_ip(BSP_DEFAULT_ENET_DEVICE, &ip_data);

                printf("\nIP Address      : %d.%d.%d.%d\n", IPBYTES(ip_data.ip));

                printf("\nIP Address HEX  : %x", ip_data.ip);

                printf("\nSubnet Address  : %d.%d.%d.%d\n", IPBYTES(ip_data.mask));

                printf("\nGateway Address : %d.%d.%d.%d\n", IPBYTES(ip_data.gateway));

                printf("\nDNS Address     : %d.%d.%d.%d\n", IPBYTES(ipcfg_get_dns_ip(BSP_DEFAULT_ENET_DEVICE,0)));

            }

        }

        else

        {

            printf("\nRTCS_Create failed !\n");

            _task_block();

        }

    }

Hope this will be useful to you.

3,315 次查看
esaias_pech
Contributor I

Hi,

 

Were you able to fix this issue? I have encountered the same problem. I am running CW10.1 and MQX3.7 (I tried with MQX 3.8 as well)

0 项奖励
回复
3,315 次查看
monXii
Contributor III

can you use the ethernet port with static ip address?

 

.. if this doesn't work check the jumper settings on the K60 and the Serial Board !