Set K60 M3 pin as VREF_OUT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Set K60 M3 pin as VREF_OUT

1,842 Views
Teckna
Contributor V

Hi,

i'm using MQX 3.8, CW 10.2 and a custom board based on K60N512.

 

I should set M3 pin of K60 as VREF_OUT mode but i don't find the way.

What are instructions to do it?

 

Can you help me?

 

Thanks!

0 Kudos
Reply
4 Replies

1,609 Views
c0170
Senior Contributor III

Hi teckna,

 

where is the problem?

Chapter 37 describes Voltage Reference and it's registers. Use bareboard approach to set registers

 

Regards,

MartinK

0 Kudos
Reply

1,609 Views
Teckna
Contributor V

Hi Kojto,

 

my problem is not setting voltage reference but how set the pin M3 for VREF_OUT configuration.

M3 pin has 4 possible configuration:

1)VREF_OUT

2)CMP1_IN5/
3)CMP0_IN5/
4)ADC1_SE18

 

It's not a PTx pin, then i can't use bit ALT to set its configuration.

 

Regards,

Teckna

0 Kudos
Reply

1,609 Views
c0170
Senior Contributor III

Hi Teckna,

 

M3 pin is dedicated output. Just leave default settings (ALT 0) and enable VREF module and necessary registers and it should be running.

 

Regards,

MartinK

0 Kudos
Reply

1,609 Views
Teckna
Contributor V

Hi Kojto,

 

in my application VREF module is disabled.

 

My VREF_OUT signal is driven by  an external voltage reference source via the VREF_OUT pin.

 

I want to be sure that in my condition M3 pin configuration is as VREF_OUT but i am not able to find its configuration register.

May  you indicate me the register?

 

Many Thanks.

 

Teckna 

0 Kudos
Reply