SPI hangs when writting in K70

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPI hangs when writting in K70

1,196件の閲覧回数
pramodk_g_
Contributor III

Hi ,     

                      I am working on a K70F120 with MQX 4.0.1.  I have an spi lcd interfaced to my board and am using spi2 for that. Whenever I  need to update some data I am sending 12K bytes to lcd via spi2. I could able to successfully display the data on LCD. But my issue arises when I am continuously updating lcd with a delay (say 1 sec) and it gets hang. When I pause the debugging i can see that It typically hangs in the files like queue.c  ( in functions like _queue_insert ).  Is this something regarding DMA issue used in spi2 or something different. If so is there anyway to disable DMA of spi2 in MQX 4.0.1. Please let me know your valuable thoughts.

Thanks,

Pramod.

タグ(3)
0 件の賞賛
返信
1 返信

1,073件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi Pramod,

That have been many enhancement to MQX4.0.1.  Will you please try MQX4.1?

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MQX&fpsp=1&tab=Design_Tools_Tab

Regards,

David

0 件の賞賛
返信