SD CARD + TWRLCD + TWRMCF52259

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SD CARD + TWRLCD + TWRMCF52259

ソリューションへジャンプ
3,023件の閲覧回数
M_ttferrari
Contributor III

HI, I'm trying to find the way to read/write an SD card on TWRLCD handled by TWRMCF52259. I'm following the sdcard example of MQX 3.6.1 (msf/examples/sdcard), the example work fine until line where it need be open with fopen("sdcard:",0) -> this function return a NULL handle, so the sd_task, then, is blocked.

 

I don't know where continue finding out... Any ideas about what it is happening??

 

Thanks 

0 件の賞賛
返信
1 解決策
2,078件の閲覧回数
M_ttferrari
Contributor III

The problem was solved setting as input with internal pullups the PORTE [4:7] of MCF51JM on TWRLCD.

 

Now the example work fine.

 

Thank you for your aswer PetrM...

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,078件の閲覧回数
PetrM
Senior Contributor I

Hello,

 

this is standard behaviour when SD card cannot be initialized (mostly due to SPI/eSDHC communication problems).

I'm suggesting to run it without TWRLCD. If that works, the problem is in SPI connections.

On twrmcf52259, the QSPI is connected to both SPI0 and SPI1 pins on elevator port B. Please check all those connections if they interfere with something on LCD board (check also LCD jumpers/switches).

 

PetrM

 

0 件の賞賛
返信
2,078件の閲覧回数
M_ttferrari
Contributor III

Hi PetrM

 

If I run it without TWRLCD I won't have a SD card Slot. 

 

LDC switch configurations are:

 

SW1/JP1=OFF, SW1/JP2=ON, SW1/JP3=ON, SW1/JP4=ON, SW1/JP5=ON, SW1/JP6=OFF, SW1/JP7=ON, SW1/JP8=OFF

 

I'm suspecting that some defines like BSP_SDCARD_GPIO_CS, BSP_SDCARD_GPIO_DETECT, BSP_SDCARD_GPIO_PROTECT and BSP_SDCARD_SPI_CHANNEL all of these define are in twrmcf52259.h, but I don't know where the project is doing refece to this file because when I search "twrmcf52259.h" inside the project I don't have any results.

 

By other hand, demo.c has some conditional compiles, one of them is #if defined BSP_SDCARD_GPIO_CS at least that I define this macro in demo.c, this conditional compilation line doesn't compile even if I include twrmcf52259.h a quite rare situation, doesn't it?

 

So, I don't know if I need BSP_SDCARD_GPIO_SC or not and, I don't know too, what is it happening with QSPI...

 

Matt

0 件の賞賛
返信
2,079件の閲覧回数
M_ttferrari
Contributor III

The problem was solved setting as input with internal pullups the PORTE [4:7] of MCF51JM on TWRLCD.

 

Now the example work fine.

 

Thank you for your aswer PetrM...

0 件の賞賛
返信